Browse FAQs

How can I determine if the RJ45 port on my Modicon M340 CPU is a Modbus or Modbus TCP/IP port ?

Published date: 08 July 2020

There are two options as listed below:
1. The port has a label printed above or below it, which will indicate either Modbus or Ethernet.
2. The port has a color coded triangle indication on the right side of it. A black triangle indicates a serial or Modbus port and a green triangle indicates an Ethernet port.


Legacy KB System (APS) Data: RESL187151 V1.0, Originally authored by DaSo on 07/18/2007, Last Edited by DaSo on 07/18/2007
Related ranges: Modicon M340

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.