Browse FAQs

What is the maximum exchange capacity of the IO Scanner serviceon the M340 NOE0100 module

Published date: 13 July 2020

For the BMX NOE 0100, the maximum IO Scanner exchange capacity of the M340 is the following:
.. read zone: 2048 words
.. write zone: 2048 words



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.