Browse FAQs

What is the difference between Momentum I/O bases 170ANR12090 and 170ANR12091?

Published date: 20 July 2020

The 170ANR12091 is similiar to the model 170ANR12090, with the exception that it has bipolar analog input and output ranges of -10 to +10 V,
The 170ANR12090 provides a unipolar range of 0-10 V,  there is no option for +/- 10V


Legacy KB System (APS) Data: RESL193347 V1.0, Originally authored by DaSo on 12/11/2008, Last Edited by DaSo on 12/11/2008
Related ranges: Modicon Momentum I/O

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.