{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
When installing Vijeo Designer on a Windows PC it says that I need to have administrator's right. How can I solve this problem?

Issue
When installing Vijeo Designer on a Windows PC it says that I need to have administrator's right. How can I solve this problem?

Product Line
Vijeo Designer

Environment
Windows Vista, Windows 7, Windows 8, Windows 10

Resolution
Typically the issues that arise in Windows can come from the UAC (User Account Control)

To help you uninstall Vijeo-Designer, you can do the following:

1) Go to the Windows Start Menu -->All Programs --> Schneider Electric --> Vijeo-Designer
2) Right-Click on the "Uninstall Vijeo-Designer" Icon
3) Select "Run as Administrator"

By doing so, this will elevate the access rights you have to the highest possible. Note that the Windows User that you are logged in as will determine the access rights in Windows. Please talk to your PC's administrator or local IT department if you do not have these rights.

Schneider Electric Global