{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Difference between the 'STBXCA1003' or 'LU9RCD03' cable.

Issue
Difference between the 'STBXCA1003' or 'LU9RCD03' cable.

Product Line
Advantys Configuration software.

Environment
Windows 7

Resolution
The pinouts for both cables are identical. The only difference is the type of connector that is used on
the end of the cable and the length of the cable. The 'LU9RCD03' uses a straight connector and an
angled connector and is 30cm long. The STBXCA1003 uses two angled connectors and is 4.5m long.


Legacy KB System (APS) Data: RESL198335 V1.0, Originally authored by AlCh on 05/04/2009, Last Edited by AlCh on 05/04/2009
Related ranges: Advantys STB

Schneider Electric Global