Browse FAQs

What is the cable pinout for the Com 1 RS485 2 wire between two Magelis XBTGC / XBTGT OR HMIGTO?

Published date: 04 November 2019


XBTGC XBTGC
XBTGT XBTGT


1--| |--1
|----------------------------| (jumped on both sides and connected across)
3--| |--3


2--| |--2
|----------------------------| (jumped on both sides and connected across)
7--| |--7



4--| |--4
| | (jumped on both sides only)
8--| |--8



6--| |--6
| | (jumped on both sides only)
9--| |--9



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.