What is the maximum number of serial communications modules, BMXNOM0200, that may be configured in an M340 system?
Published date:
27 September 2018
A M340 BMXP3420xx version 2.x processor can support a maximum of 36 Application Specific Channels.
Each BMXNOM0200 module is counted as 2 Application Specific Channels. This gives a maximum potential of 18 BMXNOM0200 modules.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.