Browse FAQs

How can I copy multiple Genie, Supergenie, Symbol and template library files between Vijeo Citect V7.2 applications.

Published date: 05 November 2018

There are following library files residing inside project folder and they can be just copied/pasted across different projects.

.CTM file  - Genie or Supergenie library
.CTL file - Symbol library
.CTT file - template library

You can copy these files from one project and can paste into another project folder where you want to use them. Make sure to then pack the project -> Pack libraries -> Update pages -> Compile project (by turning off Increment compile) to restore those files into new project.


Legacy KB System (APS) Data: RESL206763 V1.0, Originally authored by MiMe on 11/29/2011, Last Edited by MiMe on 11/29/2011
Related ranges: Vijeo Citect

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.