Browse FAQs

What is the recommended distance for installing Self Terminating F Adapter (STFA) to a splitter?

Published date: 21 October 2019

Issue:
What is the distance for the STFA to a splitter?

Product Line:
Any Remote I/O products

Cause:
Hot Standby failure if not used to replace a CRP without potential failure.

Resolution:
The allowable distance between the STFA and the splitter is 8 to 100 feet. More information on this can be found in the Remote I/O Cable System Manual 890USE10100.
 



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.