Browse FAQs

What is the part number of the cable to go from a Magelis XBTN401 to an Altivar ATV312 VFD?

Published date: 05 November 2019

Issue:
Looking for the cable that goes from the Magelis XBTN401 to the Altivar ATV312 Drive.

Product line:
Magelis XBTN401 and Altivar ATV312

Cause:
Need cable to communicate between the XBTN401 and the Altivar ATV312.

Resolution:
The part number of the cable to go from a Magelis XBTN401 to an Altivar ATV312 drive is the XBTZ938 cable.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.