Browse FAQs

What cables are available to be used with the BMXAMI0800 or the BMXAMI0810 ?

Published date: 06 December 2019

Issue:
What are the cable part numbers available for the BMAMI08xx modules?

Product Line:
M340, M580, x80 

Cause:
Need cable options for the BMXAMI0800 and 0810 I/O modules.

Resolution:
There are two types of cables, each available in two lengths.
One 28-way terminal block on one end and flying leads on the other end.
BMXFTW308S - 3 meter (flying leads)
BMXFTW508S - 5 meter (flying leads)

One 28-way terminal block on one end and one 25-way D-sub connector on the other end for sub-bases (ABE7CPA02/03/31/31E).
BMXFTA150 - 1.5 meter ( molded 25 pin D connector)
BMXFTA300 - 3 meter    ( molded 25 pin D connector)

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.