Does the 140XBE10000 Quantum backplane extender module come as a kit or are the components sold separately?
Published date:
30 April 2019
Issue
140XBE10000 sold as a kit or separately
Product Line
Modicon Quantum
Resolution
The 140XBE10000 Quantum backplane extender module are sold separately and you also need to purchase the extender cable (see below).
140XCA71703 Quantum backplane extender cable, 3 ft, 1 m
140XCA71706 Quantum backplane extender cable, 6 ft, 2 m
140XCA71709 Quantum backplane extender cable, 9 ft, 3.1 m
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.