Browse FAQs

What might cause "Connect not equal - miscompare at Word 81" when using Concept 2.6 SR2 ?

Published date: 21 October 2019



The uploaded version of the project was created from the Standby PLC. Word 81 represents the unit address, so the PLC projoct will be seens as unequal
when connecting to the Primary PLC which is using the rotory switch address rather than the offset address.
Another possibility could be that you do not have all of the appropriate patches for Concept 2.6 SR2. There are 3, patches A,B and C.
patches_abc.7zpatches_abc.7z


Legacy KB System (APS) Data: RESL211887 V1.0, Originally authored by DaSo on 06/26/2013, Last Edited by DaSo on 06/26/2013
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.