What causes error message "Unable to set clock with specified values. Clock in Error State." when using the TOD clock function in a Momentum PLC?
Published date:
27 November 2018
This error message can be caused by one of the following:
- Momentum option adapter is not present.
- Faulty option adapter.
- Are the TOD registers configured in the Specials section of the project's configuration?
- Bent pins on base/adapter/PLC?
- Reload firmware.
If the TOD registers are configured and the adapter is present, this is usually caused by bad hardware or wiring.
Legacy KB System (APS) Data: RESL211967 V1.0, Originally authored by DaSo on 07/03/2013, Last Edited by DaSo on 07/03/2013
Related ranges: Modicon Momentum
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.