Browse FAQs

What is the correct stripped exec to load into a Quantum 140CPUX130X when using Concept 2.6?

Published date: 04 May 2020

Issue:
What are the latest stripped executives for the 140CPUX1130X Quantum controllers?

Product line:
Quantum 140CPU11302, 140CPU11303, 140CPU21304

Environment:
Concept programming software

Cause:
Selecting the correct firmware to load into the Quantum controllers for IEC.

Resolution:
The PV version of the 140CPUX130X will determine what firmware you will need.

If the PV is < PV06, it is Q1SV248E.BIN.

If the PV is => PV06,  it is Q1RV301E.BIN.


Note:  The Quantum 140CPUX130x is obsolete and depending on the application the M340 or the M580 would be the replacement  and import the program into the Ecostruxure Control Expert Software ( formally Unity Pro software).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.