Browse FAQs

When wiring a BMXDAO1605 discrete output module, is the 120VAC power to each group of the module a line or neutral connection ?

Published date: 21 October 2019

Each group of the BMXDAO1605 module, should have a fused connection to the 120 VAC line . Pins 5,10,15 & 20. We recommend a 3 Amp fast blo fuse for each group.


Legacy KB System (APS) Data: RESL212608 V1.0, Originally authored by DaSo on 09/26/2013, Last Edited by DaSo on 09/26/2013
Related ranges: Modicon M340

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.