Can I use a 140NOE77100 in a ProWORX NxT Quantum Hot Standby system?
Published date:
30 January 2019
Yes. It is strongly recommended that the 140NOE77100 firmware be upgraded to v3.xx for full hot standby functionality with a ProWORX configuration.
Legacy KB System (APS) Data: RESL212671 V1.0, Originally authored by DaSo on 10/03/2013, Last Edited by DaSo on 10/03/2013
Related ranges: Modicon Quantum
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.