Browse FAQs

What is the replacement part number for the Magelis XBTGT2330 HMI?

Published date: 24 January 2019

Issue
The Magelis XBTGT2330 HMI is no longer in production. What is the replacement part number for the Magelis XBTGT2330 HMI?

Product Line
Magelis XBTGT2000 series HMI, XBTGT2330

Resolution
The three options to replace the obsolete XBTGT2330 are:

1) HMIGTO2310 (5.7" screen)
https://www.se.com/us/en/product/HMIGTO2310/advanced-touchscreen-panel-320-x-240-pixels-qvga--5.7%22-tft---96-mb/
This has the same resolution as the XBTGT2330 (320x240) and 65,536 colors, so it will only require a change in HMI ("Target") Type in the configuration software of the project.
The dimensions for mounting are the same as the XBTGT2330.
The HMIGTO series requires Vijeo Designer v6.2 (Part Number: VJDSNDTGSV62M)

2) XBTGT2390 (5.7" screen)
https://www.se.com/us/en/product/XBTGT2930/advanced-touchscreen-panel---320-x-240-pixels-qvga---5.7%22---tft-lcd---24-v-dc/
This HMI is almost exactly the same as the XBTGT2330 and is the closest replacement with newer electronics.
The dimensions are the same as the original XBTGT2330.
This has the same resolution as the XBTGT2330 (320x240) with 65,536 colors and will require NO change in the configuration project.
Just call your dealer to ensure that it can be ordered as it may be in short supply.

3) HMIG3U in combination with HMIDT351 (7" screen)
https://www.se.com/us/en/product/HMIG3U/premium-box-for-universal-panel/
https://www.se.com/us/en/product/HMIDT351/7w-touch-advanced-display-wvga/
The HMIG3U back module holds the CPU and Communication ports, while the HMIDT351 is the 7"  touchscreen that locks into the back module.
This one is higher resolution at 800x480, 262,144 colors, and has much faster processing power.
This will require a change in HMI ("Target") Type in the configuration software (Vijeo Designer v6.2) of the project as well as require object resizing in the software configuration.
This requires a larger cutout for mounting.

For reference, the XBTGT2330 product page:
https://www.se.com/us/en/product/XBTGT2330/advanced-touchscreen-panel---320-x-240-pixels-qvga---5.7%22-tft-lcd---24-v-dc/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.