{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How Do I Configure Microsoft Excel To Allow Macros To Run when running reports using Repgen?

Issue
The ION Enterprise 5/6 or PME 7/8 reporter application fails to generate a report with the following error: "Your Excel security settings do not allow this waveform processing to run."




Product Line
StruxureWare Power Monitoring Expert, Reporter

Environment
ION Enterprise 5/6, Power Monitoring Expert 7/8, Microsoft Excel 2007/2010/2013/2016

Cause
The Microsoft Excel security settings are not setup to allow trust access to the VBA project object model.

Resolution

A number of the default Reporter Excel-based reports require Trust Access to the VBA project model. Follow the steps below to change this setting within Microsoft Excel 2016. Other Microsoft Excel versions will have a similar procedure.

1. Run Micrsoft Excel.
2. Click on the 'File' tab located in the upper left corner of the window.
3. At the bottom of the pop-up menu, clidk on Options.
3. Click on the 'Trust Center' tab.
4. Click on 'Trust Center Settings'.
5. Click on 'Macro Settings'
6. Place a check-mark in the 'Trust access to VBA project model' check box within the 'Developer Macro Settings' section.
7. Rerun the report.

** Ensure that Macros are enabled within MS Excel.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.