Analog Output Specifications for I/O External Expander Module Option D of the ION8600/ION8650 meter
Issue:
Recognizing I/O of an external expander for ION8600/ION8650 meters.
Product Line:
ION8650- P850EB0
ION8600- P850EA0
Environment:
ION8650 Expander I/O Module
Cause
User couldn’t identify and wire the ION8650 meter Expander I/O module
Resolution:
Click the link for each model for more information: P850EA0/P850EB0 digital I/O expander module.
module.
- A-1 is 0 to 20 mA
- A-2 is 0 to 20 mA
- A-3 is -1 to 1 mA
- A-4 is -1 to 1 mA