{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How is the Field Calibration for the ION8650 Different than the ION8600?

Issue
How is the Field Calibration for the ION8650 Different than the ION8600?

Product Line
PowerLogic ION 8600, ION 8650

Environment
Field calibrating PowerLogic ION 8600, ION 8650 meters with ION Setup

Cause
8650: Field calibration is accomplished using a built-in firmware feature.
8600: Field calibration is accomplished using ITC modules (framework) so no firmware changes are required.

Resolution
The ION Setup Calibration Wizard realizes how it is done differently in both meters and adjusts things accordingly.

For instructions and related documents required to the field calibration of ION 8600/8650 meters,
refer to article: FA209892 - Powerlogic ION 7650/8600/8650/8800 Field Calibration Documentation

Schneider Electric Global