Browse FAQs

Where can I find the Compatibility Support Matrix for PowerLogic/PowerSCADA Expert/ION products?

Published date: 03 December 2019

Issue
Where can I find the Hardware and Software Support Matrix for PowerLogic, Power Scada Expert, and ION products?

Product Line
Power Monitoring Expert
Power Scada Expert 
ION Enterprise
Struxureware Power Monitoring
Summary Report Packs
Event Notification Module
Active Pager Module
SMS
Sequence of Events Recorder

Environment
For New Installations

Cause

Need to know what Hardware and Software Matrix support is needed to install software packages. 

Resolution

Power Monitoring Expert 9.0 Support
The Windows Operating System versions appy to 32 and 64 bit systems
 
Operating Systems
Windows 7 Professional/Enterprise (for Engineerng Clients Only)
Windows 10 Professional/Enterprise
Windows Server 2012 R2 Standard/Enterprise
Windows Server 2016 Standard
 
SQL Server Editions StandAlone Server Distributed Database Server
SQL Server 2012 Express Yes  
SQL Server 2014 Express Yes  
SQL Server 2016 Express (Included with PME 9.0) Yes  
SQL Server 2017 Express Yes  
SQL Server 2012 Standard/Enterprise/Business Intelligence Yes Yes
SQL Server 2014 Standard/Enterprise/Business Intelligence Yes Yes
SQL Server 2016 Standard/Enterprise/Business Intelligence Yes Yes
SQL Server 2017 Standard/Enterprise/Business Intelligence Yes Yes

Power Monitoring Expert 8.2 Support 
Operating Systems
Windows 7 Professional/Enterprise, SP1 32/64
Windows 8.1 Professional/Enterprise 64
Windows 10 Professional/Enterprise 64
Windows Server 2008 R2 Standard/Enterprise, SP1 32/64
Windows Server 2012 Standard 64
Windows Server 2012 R2 Standard 64
Windows Server 2016 Standard 64
 
SQL Server Editions StandAlone Server Distributed Database Server
SQL Server 2008 R2 Express, SP3 Yes  
SQL Server 2012 Express, SP3 Yes  
SQL Server 2014 Express, SP1, SP2 Yes  
SQL Server 2016 Express, SP1 Yes  
SQL Server 2008 R2 Standard/Enterprise, SP3 Yes Yes
SQL Server 2012 Standard/Enterprise/Business Intelligence, SP3 Yes Yes
SQL Server 2014 Standard/Enterprise/Business Intelligence, SP1 SP2 Yes Yes
SQL Server 2016 Standard/Enterprise/Business Intelligence, SP1 Yes Yes
 
Note that supported 32-bit and 64-bit SQL Server editions can only be installed on supported 32-bit and 64-bit Windows operating systems, respectively. For example, a 32-bit SQL Server edition is not supported on a 64-bit Windows operating system.
 

Power Monitoring Expert 8.1 Support 

Operating Systems
Windows 7 Professional/Enterprise, SP1 32/64
Windows 8.1 Professional/Enterprise 64
Windows 10 Professional/Enterprise 64
Windows Server 2008 R2 Standard/Enterprise, SP1 32/64
Windows Server 2012 Standard, 64
Windows Server 2012 R2 Standard 64
 
SQL Server Editions StandAlone Server Distributed Database Server
SQL Server 2008 R2 Express, SP3 Yes  
SQL Server 2012 Express, SP2 Yes  
SQL Server 2014 Express, SP1 Yes  
SQL Server 2008 R2 Standard/Enterprise, SP3 Yes Yes *1
SQL Server 2012 Standard/Enterprise/Business Intelligence, SP3 Yes Yes *2
SQL Server 2014 Standard/Enterprise/Business Intelligence, SP2 Yes Yes *2
 
1. Supported for a distributed database server configuration on WindowsServer 2008 R2 Standard/Enterprise SP1.
2. Supported for a distributed database server configuration on WindowsServer 2012 Standard SP1, and on WindowsServer 2012 R2 Standard.
 Note that supported 32-bit and 64-bit SQL Server editions can only be installed on supported 32-bit and 64-bit Windows operating systems, respectively. For example, a 32-bit SQL Server edition is not supported on a 64-bit Windows operating system.


Power Monitoring Expert 8.1 DCE Support

Operating Systems
Windows 7 Professional/Enterprise, SP1 32/64
Windows 8.1 Professional/Enterprise 64
Windows 10 Professional/Enterprise 64
Windows Server 2008 R2 Standard/Enterprise, SP1 32/64
Windows Server 2012 Standard, 64
Windows Server 2012 R2 Standard 64
 
SQL Server Editions
SQL Server 2008 R2 Standard/Enterprise, SP3
SQL Server 2012 Standard/Enterprise/Business Intelligence, SP2
SQL Server 2014 Standard/Enterprise/Business Intelligence, SP1

 Note: 32-bit and 64-bit versions are supported. Bites must match between SQL Server and Windows OS (32-bit SQL on 32-bit Windows, 64-bit SQL on 64-bit Windows).

Power Monitoring Expert 8.0 Support
 
Operating Systems
Windows 7 Professional/Enterprise, SP1 32/64
Windows 8.1 Professional/Enterprise 64
Windows Server 2008 R2 Standard/Enterprise, SP1 32/64
Windows Server 2012 Standard, 64
Windows Server 2012 R2 Standard 64
 
SQL Server Editions StandAloneServer  Distributed Server
SQL Server 2008 R2 Express, SP3 Yes No
SQL Server 2012 Express, SP2 Yes No
SQL Server 2014 Express, SP1 Yes No
SQL Server 2008 R2 Standard/Enterprise, SP3 Yes Yes *1
SQL Server 2012 Standard/Enterprise/Business Intelligence, SP3 Yes Yes *2
SQL Server 2014 Standard/Enterprise/Business Intelligence, SP2 Yes Yes *2
 
1. Supported for a distributed database server configuration on WindowsServer 2008 R2 Standard/Enterprise SP1.
2. Supported for a distributed database server configuration on WindowsServer 2012 Standard SP1, and on WindowsServer 2012 R2 Standard.
 Note that supported 32-bit and 64-bit SQL Server editions can only be installed on supported 32-bit and 64-bit Windows operating systems, respectively. For example, a 32-bit SQL Server edition is not supported on a 64-bit Windows operating system.
 
Power Monitoring Expert 7.2.2 Support

Operating Systems and Respective SQL installations
32-bit Windows Operating Systems 32-bit Microsoft SQL Server Editions Standalone Server Distributed Database Server
Windows 7 Professional/Enterprise, SP1 SQL Server 2008 R2 Express, SP2 Yes No
SQL Server 2008 R2 Standard/Enterprise, SP2 Yes No
SQL Server 2012 Express, SP1 Yes No
SQL Server 2012 Standard/Enterprise, SP1 Yes No
Windows Server 2008 Standard/Enterprise, SP2 SQL Server 2008 R2 Express, SP2 Yes No
SQL Server 2008 Standard/Enterprise, SP3 Yes Yes
 
64-bit Windows Operating Systems 64-bit Microsoft SQL Server Editions Standalone Server Distributed Database Server
Windows 7 Professional/Enterprise, SP1 SQL Server 2008 R2 Express, SP2 Yes No
SQL Server 2008 R2 Standard/Enterprise, SP2 Yes No
SQL Server 2012 Express, SP1 Yes No
SQL Server 2012 Standard/Enterprise, SP1 Yes No
Windows Server 2008 Standard/Enterprise SP2, and R2 SP1 SQL Server 2008 R2 Express, SP2 Yes No
SQL Server 2008 R2 Standard/Enterprise, SP2 Yes Yes
Windows Server 2012 / R2 Standard/Enterprise SQL Server 2012 Express, SP1 Yes No
SQL Server 2012 Standard/Enterprise, SP1 Yes Yes
 
Struxureware Power Monitoring 7.0.1 Support
Operating Systems and Respective SQL installations
32-bit Windows Operating Systems 32-bit Microsoft SQL Server Editions Standalone Server Distributed Database Server
Windows 7 Professional Enterprise Editions, SP1 SQL Server 2008 R2 Express Edition x
SQL Server 2008 R2 Standard Edition, SP1 x
Windows Server 2008 Standard/Enterprise Editions, SP2 SQL Server 2008 R2 Express Edition x
SQL Server 2008 Standard/Enterprise Editions, SP2
SQL Server 2008 R2 Standard/Enterprise Editions, SP1
 
64-bit Windows Operating Systems 64-bit Microsoft SQL Server Editions Standalone Server Distributed Database Server
Windows 7 Professional Enterprise Editions, SP1 SQL Server 2008 R2 Express Edition x
SQL Server 2008 R2 Standard Edition, SP1 x
Windows Server 2008 Standard/Enterprise Editions, SP2 SQL Server 2008 R2 Express Edition x
SQL Server 2008 Standard/Enterprise Editions, SP2
SQL Server 2008 R2 Standard/Enterprise Editions, SP1
Windows Server 2008 R2 Standard/Enterprise Editions, SP1 SQL Server 2008 R2 Express Edition x
SQL Server 2008 Standard/Enterprise Editions, SP2
SQL Server 2008 R2 Standard/Enterprise Editions, SP1
 
ION Enterprise 6.0 SP1 Support
Operating Systems and Respective SQL installations  
32-bit Microsoft Windows Operating Systems 32 bit Microsoft SQL Server Versions StandAlone Distributed DB Server  
Windows XP (32-bit) Professional Edition, SP3 SQL Server 2005 (32-bit) Express Edition from the ION:E DVD x  
Windows Vista (32-1,4) Business/Ultimate/Enterprise Editions, SP2 SQL Server 2005 (32 bit) Express Edition from the ION:E DVC x  
Windows 7 (32-bit) Professional/Enterprise Editions SQL Server 2005 (32-bit) Express Edition from the ION:E DVD 1 x  
SQL Server 2005 (32 bit) Standard/Enterprise Editions 2 x  
SQL Server 2008 R2 (32 bit) Standard/Enterprise Editions 3 x  
Windows Server 2003 (32-bit) Standard/Enterprise Editions, SP2 SQL Server 2005 (32-bit) Express Edition from the ION:E DVD x  
SQL Server 2005 (32-bit) Standard/Enterprise Editions  
Windows Server 2003 R2 (32-bit) Standard/Enterprise Editions SQL Server 2005 (32-bit) Express Edition from the ION:E DVD x  
SQL Server 2005 (32-bit) Standard/Enterprise Editions  
Windows Server 2008 (32-bit) Standard/Enterprise Editions, SP2 SQL Server 2005 (32-bit) Express Edition from the ION:E DVD x  
SQL Server 2005(32-big Standard/Enterprise Editions  
SQL Server 2008 R2 (32-big Standard/Enterprise Editions 7 11  
   
64 bit Microsoft Windows Operating Systems Microsoft SQL Server Versions  StandAlone Distributed Minimalist
Windows 7 (64-bit) Professional/Enterprise Editions SQL Server 2005 (32-bit) Express Edition from the ION:E DVD 4 x x
SQL Server 2005 (64-bit) Standard/Enterprise Editions 5 x x
SQL Server 2008 R2 (64-bit) Standard/Enterprise Editions 6 x x
Windows Server 2008 64 bit Standard/Enterprise Editions, SP2 SQL Server 2005 (32-bit) Express Edition from the ION:E DVD 8 x x
SQL Server 2005 (64-bit) Standard/Enterprise Editions 9 12 x
SQL Server 2008 R2 (64-bit) Standard/Enterprise Editions 10 13 14
Windows Server 2008 R2 64 bit Standard/Enterprise Editions SQL Server 2005 (32-bit) Express Edition from the ION:E DVD 8 x x
SQL Server 2005 (64-bit) Standard/Enterprise Editions 9 12 x
SQL Server 2008 R2 (64-bit) Standard/Enterprise Editions 10 13 x

 Browser Support for ION E, Struxureware Power Monitoring, and Power Monitoring Expert Support​​​​​​​
Browser Support for ION/SPM/PME
Browser Support  ION E 6.0 SPM 7.0.1 PME 7.2.2 PME 8.0 PME 8.1 PME 8.2 PME 9.0
IE 11      
IE 10      
IE 9          
IE 8          
IE 7            
IE 6            
Chrome 16+              
Chrome 20 or later            
Chrome 42 and later*      
Firefox 14+              
Firefox 35 and later*      
Microsoft Edge*        
Safari 5 and later            
Safari 7 and after      
Safari 8 and after            

* The browsers support the web application framework, and Dashboards, Diagrams, and Trends
applications. Alarms and Tables are dependent on browser support of the Silverlight plugin.

Power Scada Expert Support​​​​​​​
Operating Systems PLS 7.10 PLS 7.20 PSE 7.30 PSE 7.40 PSE 8.0 PSE 8.1 PSE 8.2 PSE 9.0
Windows XP, SP3 Professional Yes Yes Yes No No No No No
Windows Server 2003, SP2 Standard/Enterprise Yes Yes Yes No No No No No
Windows Server 2003 R2, SP1 Yes Yes No No No No No No
Windows Vista, SP2 Yes Yes Yes No No No No No
Windows 7, SP1 Professional/Enterprise No Yes Yes Yes Yes Yes *4 Yes *4 Yes *5
Windows Server 2008, SP2 Standard/Enterprise No Yes Yes Yes No No No No
Windows Server 2008 R2, SP1 No Yes Yes Yes Yes Yes Yes No
Windows 8 No No Yes *1/2 Yes Yes Yes *4 Yes *3/4 No
Windows 8.1 No No No No Yes *2 Yes *4 Yes *4 No
Windows Server 2012 No No Yes *1/2 Yes Yes Yes Yes Yes
Windows Server 2012 R2 No No No No Yes *2 Yes Yes Yes
Windows 10 No No No No No No Yes *4 Yes *5
Windows Server 2016 No No No No No No Yes Yes
 
1. Service Pack 1 for the operating system is required
2. Available with PowerSCADA Expert Service Release 1
3. Not supported by Advanced Reporting and Dashboards (PME)
4. Not supported by PowerSCADA Anywhere
5. Support for 64-bit Windows only


Summary Report Pack Support  
Platform Compatibility      
✓=Supported SRP 2.1 SRP 3.0  SRP 3.0.1 SRP 3.2 SRP 4.0  SRP 4.2 SRP 4.3 SRP 5.1 SRP 5.2 SRP 6.0
ION Enterprise 6.0 SP1 x x x x x x x x x
SPM 7.0 x x x x x x x
SPM 7.0.1 x x x x x x x x
PME 7.2 x x x x x x x x
PME 7.2.1 x x x x x x x x
PME 7.2.2 x x x x x x x x
PME  8.0 x x x x x x x   x
PME 8.2 x x x x x x x x x
PME 9.0 x x x x x x x x x
       
SQL Server                    
Microsoft SQL Server 2005 (32-bit) x x x x x x      
Microsoft SQL Server 2008 (32-bit & 64-bit) x x      
Microsoft SQL Server 2008 R2 (64-bit)      
Microsoft SQL Server 2008 R2 Express x x x x      
Microsoft SQL Server 2012 AI x x x x      

 Sequence of Events Recorder (SER) Support​​​​​​​
Devices SER 8.0 SER 7.5/7.5.1 SER 7.3
CM4000 (SER and Standard Alarms)
Multilin (489, 745, 750,760)
Sepam (20 40 80)
Sepam (1000 2000) x x
Moghnahan Protime
Moghnahan PLC
Cyber Sciences 3200
Cyber Sciences 2408    
Power Meter 870
Schweitzer Devices (300G,351A,700G,710,75 A) x x
Historian SER 8.0 SER 7.5/7.5.1 SER 7.3
Event Logging
"Live" Current Events view
"Historical" Events View
Event Sorting and Filtering for analysis
System Health x x x
"Live Current Events view
Historical" Events View
Event Sorting and Filtering for analysis
Operating System SER 8.0 SER 7.5/7.5.1 SER 7.3
Windows Server 2012/2012 R2 x x
Windows 8/8.1 x x
Windows Server 2008 R2 (64bit)
Windows Server 2008 (64bit)
Windows Server 2008 (32bit)
Windows 7 (64bit)
Windows 7 (32bit)
Windows Server 2003 x x
Windows Vista (32bit) x x
Windows XP x x
SQL Server SER 8.0 SER 7.5/7.5.1 SER 7.3
Microsoft SQL Server 2012 x x
Microsoft SQL Server 2008 R2 (64bit) x
Microsoft SQL Server 2008 R2 (32bit) x
Microsoft SQL Server 2008 x
Microsoft SQL Server 2005 (32bit) x x
Browser Support SER 8.0 SER 7.5/7.5.1 SER 7.3
lE 11 x x
IE 10 x x
IE 9 x x
IE 8 x x x
IE 8 (Compatibility Mode) x
Chrome 16+ x x
Firefox 14+ x x
Languages SER 8.0 SER 7.5/7.5.1 SER 7.3
English
 
*SER 7.5.1 contains the same feature set at SER 7.5, but includes a hotfix related to installs on distributed systems.              
 
Event Notification Module Support
 
Platform ENM 8.3 ENM 8.2 ENM 8.0 ENM 7.1 ENM 7.0 ENS 6.4
PME 9.0 x x x x x
PME 8.0 x x x x x
PSE 8.0 x x x x x
PSE v7.40 SR1 x x x x
PSE v7.40 x x x x
PLSCADA v7.20 x x
PLS v7.20 SR1 x x x
PSE 7.30/SR1 x x x
PLSCADA v7.10 x x x x x x
CitectSCADA v7.20 x x x x x x
CitectSCADA v7.10 x x x x x x
Vijeo Citect v7.20 x  
Vijeo Citect v7.10 x x x x x x
SPM 7.0/7.0.1 x x
PME 7.20 x x x
ION Enterprise 6.0/6.0 SP1 x x x x
SMS 4.3 x x x x x
 
Operating System ENM 8.3 ENM 8.2 ENM 8.0 ENM 7.1 ENM 7.0 ENS 6.4
Windows Server 2012 R2 (64bit) x x x x
Windows Server 2012 (64bit) x x x x
Windows Server 2008 R2 (64bit) x
Windows Server 2008 (64bit) x
Windows Server 2008 (32bit)
Windows 8.1 (64bit) x x x x
Windows 8 (64(bit) x x x x
Windows 7 (64bit) x
Windows 7 (32bit)
Windows Server 2003 x x x x x
Windows Vista (32bit) x x x x x
Windows XP x x x x x
 
Operating Systems Support for Event Notification Module
SQL Server ENM 8.3 ENM 8.2 ENM 8.0 ENM 7.1 ENM 7.0 ENS 6.4
SQL Server 2014 Standard/Enterprise x x x x x
SQL Server 2014 Express x x x x x
SQL Server 2012 Standard/Enterprise x x
SQL Server 2012 Express x x x x x
SQL Server 2008 R2 (64bit) x
SQL Server 2008 R2 (32bit)
SQL Server 2008  x x x x
SQL Server 2008 SP2 x x x x x
SQL Server 2005 (32bit) x x x x x
 
Browser Support for Event Notification Module
Browser Support ENM 8.3 ENM 8.2 ENM 8.0 ENM 7.1 ENM 7.0 ENS 6.4
IE 11 x x x
IE 10 x x x
IE 9 x x x
IE 8 x x x x x x
IE 8 (Compatibility Mode) x x x
Chrome 20+ x x x x
Chrome 16+ x x x x
Firefox 14+ x x x

System Manager Software (SMS) 4.3 Support  
32-bit Microsoft Windows Operating Systems 32-bit Microsoft SQL Server Versions Supported?
Windows XP (32-bit) Professional Edition, SP3 SQL Server 2005 (32-bit) Standard/Enterprise Yes
Windows Vista (32-bit) None No
Windows 7 (32-bit) - Professional/Enterprise  None No
Windows Server 2003 (32-bit) - Standard/Enterprise Editions, SP2 SQL Server 2005 (32-bit) Standard/Enterprise Yes
Windows Server 2003 R2 (32-bit) - Standard/Enterprise Editions SQL Server 2005 (32-bit) Standard/Enterprise Yes
Windows Server 2008 (32-bit) - Standard/Enterprise Editions, SP2 SQL Server 2005 (32-bit) Standard/Enterprise Yes
 
64-bit Microsoft Windows Operating Systems Microsoft SQL Server Versions Supported?
Windows Vista (64-bit) None No
Windows 7 (64-bit) - Professional/Enterprise Editions None No
Windows Server 2008 (64-bit) - Standard/Enterprise Editions, SP2 None No
Windows Server 2008 R2 (64-bit) - Standard/Enterprise Editions None No
 
1. Supported for a distributed database server configuration on WindowsServer 2008 R2 Standard/Enterprise SP1.
2. Supported for a distributed database server configuration on WindowsServer 2012 Standard SP1, and on WindowsServer 2012 R2 Standard.
Note that supported 32-bit and 64-bit SQL Server editions can only be installed on supported 32-bit and 64-bit Windows operating systems, respectively. For example, a 32-bit SQL Server edition is not supported on a 64-bit Windows operating system.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.