{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
The ION7500RTU meter does not accept the .dcf meter template file via ION Setup and returns the error message "Unable to download dcf(xml) file to a non-RMP device"

Goals and Symptoms

When sending the .dcf meter template file into the meter using ION Setup, it will return an error message and say "Unable to download dcf(xml) file to a non-RMP device"

Causes and Fixes

Rapid Meter Programming (RMP) is not supported in ION7500RTU meters, hence the .dcf files can not be sent to the meter using ION Setup. Instead, simply paste the .fwn version of the meter template file using ION Setup. ION Setup will treat this fwn file the same as the .dcf file with meters that support RMP. Please see the template file attached.

Attachments

(Removed File URL: 198385_B79E/7500-RTU_V1.1.0.fwn)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f23cc1f31e56d096c12575a70052a263/fl_block_5/0.56E?OpenElement&FieldElemFormat=gif)
(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f23cc1f31e56d096c12575a70052a263/fl_block_5/0.26EE?OpenElement&FieldElemFormat=gif)
Date Created: March 3, 2009
Last Revised: April 29, 2009
Public
Original Author: KG
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198385 V1.0, Originally authored by MiNe on 04/29/2009, Last Edited by MiNe on 04/29/2009
Related ranges: ION75X0 RTU, ION Setup 2.2, ION Setup 2.1

Schneider Electric Global

Attachment(s)
7500-RTU_V1.1.0.fwn [311.72 KB]