{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the ID number of Ethernet enabled ION meters for PowerLogic SCADA?

Issue
ID number is not known for ION Meters connected by Ethernet in  Power Scada Expert

Product Line
Power Scada Expert 7.20
Power Scada Expert 7.40
Power Scada Expert 8.0

Environment
Power Scada Expert with Ethernet connected ION meters

Cause
ID number is not known

Resolution
Try 255 or 100 for the ID number. One of these is likely to work since ION devices default to one or the other of these two numbers.

Schneider Electric Global