What do I need to connect the TSXETG1010 module to a Unitelway bus?
Published date:
10 May 2019
Issue:
What is needed in order to connect the TSXETG1010 module to a Unitelway bus
Product Line:
TSXETG1010, Unitelway
Resolution:
To connect the TSXETG1010 module to a Uni-Telway bus, you need one of the following:
- The cable with product reference TSX ETZ CDN 003, supplied with the module, to establish a connection via a TSX P ACC01 box,
- The cable with product reference VW3A8306 to establish a connection via a TSX SCA 62 box,
- The cable with product reference VW3A8306D30 to establish a connection via a TSX SCA 50 box.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.