Browse FAQs

How can I reset an XBTGT1xxx series password?

Published date: 31 October 2019

You need to do a recovery. If you forgot the download security password in an XBTGT1xxx series. This will erase the existing project on the XBTGT.
Procedure to do a recovery:

1) Save current project and shut-down Vijeo Designer

2) Launch the Runtime installer. Start -> Program -> Schneider Electric -> Vijeo-Designer ->Tools -> Runtime Installer

The XBTZG915 or the XBTZG925 (USB) cable is required.



3) Select the proper terminal type and check Recovery

4) Click the Send button and power cycle the XBTGT1xxx terminal



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.