Browse FAQs

What are the features in the Magelis XBT-GT which requires a CF card?

Published date: 30 October 2019


The following features in the Magelis XBT-GT requires a CF card:

1) Web Gate
2) Data Logging
3) Include Editor Project (Project Backup on HMI)
4) Download (File System)
5) Recipes (only when DownloadTo property is set to Secondary Drive)
6) Alarm Save To File
7) Data Files (only when DownloadTo property is set to Secondary Drive) this includes: Browser Files, Sound Files, Text Files, and Video Files
8) Screen Snapshot feature
9) Video (only for Target types which support video)



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.