Browse FAQs

What are the features supported by the USB Drive on the Magelis XBT-GT 2000 series and higher?

Published date: 30 October 2019


- Data logging
- Download to file system (only if the runtime on XBT GT is in version 4.6)
- Alarms "save to file"
- Screen snapshots
- Video sequences recorded during runtime



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.