Browse FAQs

How can I disable the ESC key on a Magelis XBT-R410

Published date: 31 October 2019

You need to use the System keys locking in the XBTL1000 Dialog Table.
Bit 9 disable the ESC key. Simply write a value of 0200h to that word from the PLC and it will disable the ESC key on the Magelis XBT-R410



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.