Goals and Symptoms
What does the message - Circuit Trip - mean on a Sepam Relay Series 20/40/80? |
Causes and Fixes
The Circuit Trip is related to the CB control features. It indicates that the Input I11 or input I12 on Sepam is not receiving a signal. If you are not using a Circuit Breaker control the recommendation is not to use this function.
**************************
Original article#3619
Re-published to revised security level: 17 June 2008 by DRM
Public
All content © 1992-2007 Schneider Electric
**************************
Legacy KB System (APS) Data: RESL185670 V2.0, Originally authored by KBAdPM on 06/29/2007, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20
AEDL3
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20
AEDL3