{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Update device type fails in the Modbus Device Importer (MDI) in ION Enterprise v5.5 or v5.6 when a default template is copied or modified.

Goals and Symptoms

When using a default MDI template, such as 6200.ion, as the basis for creating a new template, updating the device type fails.

Causes and Fixes

Create the device type new and the MDI will allow the device type to be added and updated. This issue has been resolved in ION Enterprise 5.6 Service Pack 1 (SP1) and above.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/589ddab5f897ef1ac125757c00162405/fl_block_5/0.2FFA?OpenElement&FieldElemFormat=gif)


  • Date Created: December 22, 2008
    Last Revised: March 16, 2009
    Public
    Original Author: MC
    All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL198053 V1.0, Originally authored by KBAdPM on 03/17/2009, Last Edited by KBAdPM on 03/17/2009
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.