{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
170AMM11030 Analog Outputs May Not Function Properly.

Issue
The purpose of this Resolution is to inform users of 170AMM11030 Momentum I/O bases of a problem with the analog outputs after operating for a short time.

After 3-4 minutes of module operation, the actual analog outputs for channels 1 & 2 are different from their expected values. Negative output voltages may occur when a positive voltage is expected.


Product Line
Momentum
170AMM11030


Resolution
A firmware and hardware solution has been implemented. Modules with an SV of 1.12 and a PV04 have this fix (implemented 9/04).

This is not a field upgradable option. Modules that are experiencing the issue described above must be exchanged.


Legacy KB System (APS) Data: RESL164814 V2.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum I/O

Schneider Electric Global