{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Memory and logging calculation tool spreadsheet for ION Meters

Issue:
User would like to know the logging capabilities of their ION meter. Such as the amount of days it would take to fill up a meter log or the max depth the log can handle based on the amount of channels, memory size, and logging interval.

Product Line:
ION7650/7550, ION8650, and ION7600/7500

Environment:
Data Logging

Resolution:
Please see the chart below as well as the excel spreadsheet below. The user can change the parameters that are highlighted in grey to suit their needs. The Configured value shows how much total memory you are using. This value cannot exceed the max amount of memory for your meter. Different meters will have different capacities.



Here is a look at the kind of calculations you can do using this spreadsheet calculation tool:

Excel example


Schneider Electric Global

Attachment(s)
Memory_and_logging_calculation_tool_spreadsheet_for_7550_or_7650.xls [20 KB]