Browse FAQs

What is the part number for the power terminal block for the ATV61/71 Frame size 8 drive?

Published date: 13 May 2019

Issue:
What is the part number for the power terminal block for the ATV61/71 Frame size 8 drive?

Product Line:
Altivar ATV61 and ATV71 frame size 8

Environment:
All

Cause:
Inter connection sub assembly connection

Resolution:
The part number is VZ3N1311 and can only be ordered thru Field Services.  
The part number is for the inter connection sub assembly. Included in this part number are the bus bar for the output phases and the input phases, the DC link Bus and the warning labels.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.