Browse FAQs

What Cablefast block can be used with the 140DRA84000 relay card?

Published date: 02 April 2020

Issue:
Can Cablefast blocks be used with the Quantum relay cards?

Product Line:
Quantum, Cablefast

Cause:
To see if we can use Cablefast with the Quantum relay modules.

Resolution:
The only block that can be used is the 140CFA04000 block and it is a straight through block. The only limitation on it is that you can not exceed .5 amps per point.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.