Browse FAQs

What are the differences between the ATV31 and ATV312?

Published date: 20 May 2020

Issue:
ATV31 vs ATV312 drive. 

Product Line:
ATV31, Altivar 31, ATV312, Altivar 312

Environment:
All models, all serial numbers.

Cause:
ATV31 became obsolete in Dec 2010.

Resolution:
The ATV312 drives are a direct replacement for the ATV31 drives (or ATV31-A). Please see attachment. The ATV312 drive has the same dimensions, wiring, and programming as the old version ATV31 drive.

The changes made from the ATV31 to ATV312 include:
-  Optional DeviceNet, Profibus, CanOpen Daisy Chain communication cards.
-  Addition of a rotary dial to quickly scroll parameters
-  Addition of Run/Stop buttons
-  Addition of a door to cover the buttons against accidental contact
-  changed the color of the plastic to follow Schneider Electric color coding (white = control section, black = power section)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.