When do I change the Unit ID of Modbus/TCP equipment from 255 to a specific value in Vijeo Designer?
Published date:
29 March 2019
Title
When do I change the Unit ID of Modbus/TCP equipment from 255 to a specific value in Vijeo Designer?
Issue
Customers that arehaving the Magelis communicate to a Modbus/TCP to Modbus/RTU devices.
Product Line
Vijeo Designer, Magelis HMI
Environment
Cause
Resolution
If you are using a Modbus/TCP to Modbus serial RTU Gateway device, each device on the serial network will have a Modbus slave address associated with that device. That Modbus slave address is your Unit ID.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.