Browse FAQs

How are preset speeds set up on the ATV312 drive?

Published date: 15 May 2020

Issue:
Preset speeds on the ATV312 drive.

Product Line:
Altivar 312

Environment
:All

Cause:
Preset speeds

Resolution:
Preset speed function can be assigned two ways to Altivar 312. 1) Logic inputs  2) Communication networks.
1)Through Logic inputs-To assign preset speeds to altivar range of drives follow below path while operating JOG dial.RDY--> Fun [Application Function]-->PSS- [Preset Speeds] -->PS2 [2 Preset speeds] = LIx. Here x refers to the available logic inputs number.When this particular LIx is ON, SP2 (preset speed 2) reference will be considered.Similarly, PS4, PS8 and PS16 can also be assigned to LIx to activate 4 preset speeds, 8 preset speeds and 16 preset speeds operation respectively.2)Through communication networksRDY-->CtL [Command Menu]-->LAC [Access Level]] = L3 [Level 3].
Assign any one bit from bit 11th to 15th of control word of particular communication network on which ATV312 is being used to preset Speeds (PS2, PS4, PS8 or PS16). Communication network could be one out of Modbus, CANOpen, DevicNet or Profibus.When assigned bit of control word is HIGH, corresponding preset speed function (PS2, PS4, PS* or PS16) will be activated and accordingly SP2 to SP16 will come into effect.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.