Browse FAQs

Are the Altivar ATV32/ATV320 drives repairable?

Published date: 20 November 2019

Issue:
Can the Altivar ATV32/ATV320 drives be repaired?

Product Line:
ATV32 ATV320

Environment:
All

Cause:
None

Resolution:
There are no repair parts for the ATV32/ATV320 drives, except for Heatsink Fan(s).  However, if the drive is out of warranty, you can contact the repair depot at 1-800-950-9550 to see if they can repair it.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.