{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What processor are used in the Preventa XPSMF35 Safety controller?
Issue
What processor are used in the Preventa XPSMF35 Safety controller

Product Line

XPSMF35

Resolution

The XPSMF35 controllers are equipped with 2 microprocessors for the safety-related processing (CPU) and 1 microprocessor for the communications (COM).

The CPU and COM Processors are 32-bit processors.

CPU: Motorola Coldfire MCF 5206e

Clock Speed: 40 MHz / 36 MIPS (54 Mhz / 50 MIPS)

COM: Motorola Power PC 860

Clock Speed: 50 MHz / 66 MIPS (66 Mhz / 88 MIPS)

Schneider Electric Global