{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to delete the buffer contents or events in the BMXNOR0200 module configured as Server in IEC Protocol, when the communication between the server and client is not present.
Issue: The customer wants to delete the buffer of BMXNOR0200

Product Line: BMXNOR0200 V1.6 & V1.7

Environment: Unity Pro V12 installed on Windows 7 Pro

Resolution:

It is not possible to delete the buffer contents or events in the BMXNOR0200. When the module configured as Server in IEC Protocol and the communication between the server and client is not present.

Schneider Electric Global