Where is a remote auto start contact terminated in an 8839 E-Flex?
Published date:
21 January 2019
Issue:
Where do I land my auto start contact in an 8839 E-Flex?
Product Line:
8839 E-FLEX
Environment::
All units with A07 or B07 modification options
Cause:
None
Resolution:
The HOA switch requires a user supplied dry contact for AUTO start/stop control. Wire the contact between terminals 7 and 6 of the DIN mounted terminal blocks.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.