Browse FAQs

Can I change the projects directory in Vijeo Designer V6.2?

Published date: 30 October 2019

No.  THe project directory is specified during the installation of Vijeo Designer V6.2.  The only way that it can be changed is by re-installing Vijeo Designer V6.2 and specifing a new directory.  It is recommended to backup the Vijeo-Manager directory folder in that process.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.