{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can an ATV212 24Vdc power supply from P24 be used for logic inputs on another ATV212 drive?
Issue:
P24 vdc signal from one ATV212 drive to start another ATV212 drive

Product Line:
Altivar ATV212

Environment:
All

Cause:
Needs to use only one power signal to start two drives.

Resolution:
Yes.  Jumper together a CC terminal from both drives so that they both have the same ground reference.
Note:  The P24 power supply is limited to 200mA.  Each logic input consumes about 5mA.

Schneider Electric Global