What is the Device Control Block used for in Unity when configuring IO Scanner?
Published date:
30 November 2018
Title
Device Control Block functionality
Issue
Usage of the Device Control Block
Product Line
M580 M340 Quantum
Environment
Unity Pro
Resolution
The Device Control Block is a flat address array of 8 contiguous words with each bit representing an entry in the I/O scanner for up to 128 logical device entries. With the bit set to 0, the IO Scanner operates for that entry. With the bit set to 1, that particular IO Scanner entry is disabled, and the Health bit (on supported controllers), is set to 1, representing an unhealthy state. This allows the developer to turn on or off individual IO Scanner entries based upon the state of each IO Scanner table entry bit.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.