In Vijeo Designer 6.2 If I use the set bit function in an Action how long will the bit stay on?
Published date:
31 October 2018
The bit must be reset by an Action or other function in the Vijeo Designer program. It will also reset if the HMI is power cycled and you do not have the retentive property set to enabled for the variable you are setting with the action.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.