Why is Proworx 32 looking for a .mdb file and giving me error # 3024 when I open a .pwx project file?
Published date:
29 March 2019
Issue
Cannot open Proworx 32 .pwx project file
Product Line
Proworx 32
Cause
When a Proworx 32 .pwx project file name is changed in Windows Explorer rather than in Proworx you will get error #3024 when trying to open the project.
Resolution
To resolve the issue the project file name needs to be changed back to the original name. If the name is not known, the project can be opened in notepad to reveal the original file name. Change the file name back to the original name in Windows Explorer. Once the name is changed back, the project should open in Proworx.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.