{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do the NetShelter 2-post or 4-post racks have castor kits available?

Issue:
Castors allow racks to move easily.

Product Line:
NetShelter SX Racks

Environment:
All versions and serial ranges.

Cause:
The NetShelter 2-post and 4-post racks don't show castor kits available as an accessory.

Resolution:
We do not offer castor kits for the 2-post or 4-post racks. The racks do have a hole in the mounting bracket that castors could be attached to, but we don't provide them. The holes in the mounting bracket is designed to be used to mount the rack to the floor.
If an a open frame rack design with castors is required please consider AR3100X617. This is a NetShelter SX with no sides or doors.

Schneider Electric Global