{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
BMXNOE0110 PV11 Firmware Compatibility Issue
Issue
This Resolution explains a firmware compatibility issue with the BMXNOE0110 at PV11.



Product Line
BMXNOE0110



Resolution
Component obsolescence required a replacement part for the BMXNOE0110's.  Modules with the new flash component are identified as PV11, which resulted in a new firmware version 5.9.

  • BMXNOE0110's at PV11 or higher are only compatible with firmware versions 5.9 or higher.
  • BMXNOE0110's at PV11 or higher cannot be downgraded with firmware versions lower than v5.9.
  • BMXNOE0110 firmware version 5.9 and higher are compatible with all BMXNOE0110 PV versions.

Schneider Electric Global