Browse FAQs

Which ATV61 / ATV71 drives are frame size 8?

Published date: 24 June 2020

Issue:
Frame size 8 ATV61 / ATV71 drives.

Product Line:
ATV61 ATV71

Environment:
All 460V/480V

Cause:
Possible alternatives

Resolution:
The following drives are rated for frame size 8.  

ATV71HD45N4, ATV71HD55N4, ATV71HD75N4
ATV61HD45N4, ATV61HD55N4, ATV61HD75N4

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.